N/A
VLT® Drives
> Products
> Drive Configurator
> Documentation
> Software Downloads
> Service & Support
> Industries We Serve
> Case Stories
> News & Press
> About ...
> How to ...
 
 
 
 
 
Danfoss Logo

VLT® drives optimise oil production in Texas

At an oil well in Texas VLT® drives maintain an optimum pressure balance between oil wells and surrounding reservoirs. More oil flows into the wells, thereby raising overall production.

Using a VLT® drive to vary the speed of certain parts of the stroke can minimize this stress, making the components last longer. This can be accomplished while still maintaining the same number of strokes per minute, which keeps production up.

Clean cut – safe cut

The PLASCUT 591 from cutter specialist MAGURIT uses the VLT® AutomationDrive with its ”Safe Stop” feature to ensure the speedy and safe opening of blood plasma packages.

Drugs and vaccines based on blood and blood plasma are crucial in the treatment of many illnesses or injuries, such as bleeding disorders, immune system deficiencies or extensive skin injuries. Therefore, all handling of blood related products needs to take place under controlled, clean and safe conditions.

High tech suture material for the medical industry in Korea and Japan

According to Managing Director Richard Slack “We selected the new Danfoss VLT® AutomationDrive for a number of reasons. In addition to the accurate vector control, there are a number of features on the AutomationDrive that simplified their adoption and gave us confidence to meet the demands. Not least of these is the ability to connect the drives on an Ethernet network, which enables us to interrogate the machine set-up remotely."

Passion and responsibility

Based on our core values, Danfoss’ vision is to be a global market leader within our core businesses: Refrigeration & Air Conditioning, Heating & Water and Motion Controls.

We aim to meet the expectations of our stakeholders by being a highly respected company, improving quality of life by mastering advanced technologies in customer applications, while focusing on environmental and social responsibility.